CPC
CPC CPC
  • Brand Overview
    • Vision
    • Mission
    • Key Messages

General Guidelines

  • Logos
    • Lockup
    • Color
    • Clear Space
    • Symbol as Art
    • Sonic Logo
  • Color
    • Primary Palette
    • Neutral Palette
    • Hierarchy
  • Typography
    • Primary Typeface
    • Alternate Typeface
    • Hierarchy
    • Example
  • Graphic Elements
    • Gradient
    • Special Use Gradient
    • Wireframes
    • CAD Drawings
    • Product Images
  • Examples
    • Digital Advertising
    • Print Ads
    • Ads with Photography

Resources

  • Downloads
  • CPC Adobe Creative Cloud

Logos

Thermal Brand Guide | CPC

 

Logos

Lockup

The preferred version of our signature includes our parent company, Dover. Always use the full signature unless it is of a size that diminishes legibility of the Dover identity, in which case the non-tagged version is approved for use.

 

Full logo with Dover tag (preferred)

Use until length is less than 2.5"

 

Without Dover tag

Logos

Color

The primary CPC signature colors are composed of 4-color blue gradation and black. The dark mode version of this logo features a blue to white gradient, white and the CPC Thermal Mint color. Consistent use of these distinctive colors reinforces a unified identity and makes the CPC signature more memorable and recognizable.

These signature colors should be used whenever possible. If 4-color is not an option, it is acceptable to reproduce the signature in 2-color or black. The signature may also be reversed as white out of a dark background.

Style Endorsed Non-Endorsed
Light Mode Download Download
Light Mode:
Black
Download Download
Light Mode:
Reverse White
Download Download
Dark Mode Download Download

Logos

Clear Space

To ensure visual impact and clarity, white space must surround the signature — without the intrusion of other graphic elements or text. The minimum amount of space surrounding our signature should be no less than the height of the letter “C” in the name, CPC. In certain circumstances, the logo may sit on top of CPC brand elements, such as wireframe graphics. In these cases, the wireframe or other graphic element must have an opacity level set low enough and a high visual contrast as to not disrupt the integrity of the logo.

 

Clear space measurement

Logos

Symbol as Art

The fluid symbol may be used alone in limited situations, such as on special premium items. It may also be used for items displayed in close proximity to other materials with the full CPC signature – such as a banner above a trade show display – or if the full signature appears elsewhere on the same surface.

 

 

Not acceptable uses

Logos

Sonic Logo

Our sonic logo reinforces our brand attributes of connection, confidence, assurance with the click, It should be used to build out recognizable brand assets whenever possible.

The sonic logo provided here should be featured on all CPC produced assets with sound.

The animated sequence with audio, featuring our sonic logo (see .mp4) should be a staple feature in all videos that include audio (voiceover or music), the animation should be standard across all videos closing scenes.

File Type Preview
Microsoft's Windows-based audio file.wav Download
Apple's QuickTime® audio file.mov Download
Logo animation + audio video file.mp4 Download

Logos

Examples -WIP

TBD

© 2026 Colder Products Company®. All Rights Reserved