CPC
CPC CPC
  • Brand Overview
    • Vision
    • Mission
    • Key Messages

General Guidelines

  • Logos
    • Lockup
    • Color
    • Clear Space
    • Symbol as Art
    • Sonic Logo
  • Color
    • Primary Palette
    • Neutral Palette
    • Hierarchy
  • Typography
    • Primary Typeface
    • Alternate Typeface
    • Hierarchy
    • Example
  • Graphic Elements
    • Gradient
    • Special Use Gradient
    • Wireframes
    • CAD Drawings
    • Product Images
  • Examples
    • Digital Advertising
    • Print Ads
    • Ads with Photography

Resources

  • Downloads
  • CPC Adobe Creative Cloud

Examples

Examples

Digital Advertisement

Banner Ads with Product

This style is characterized with the product sitting cleanly on a wireframe background and white background with the copy following the standards mentioned in the typography section.

If a single word is used on the second line, make it bold and CPC Light Blue. Otherwise, choose a word of most importance and do the same. The body copy is Trade Gothic Light in CPC Dark Gray. The rest of the copy should follow the standards mentioned in the typography section.

Use the CPC 4 color logo on the left and the button on the right.

Example of banner ad with product

Banner Ads without Product

This style is characterized with type sitting cleanly on a wireframe and white background. The copy should follow the standards mentioned in the typography section.

Choose the most important word of the headline and make it bold and use CPC light blue to highlight it.

Align all type with the center and stack it in the order as shown: 4 color logo, Headline, CTA/Button.

Button Styles

For digital ads, use a rounded rectangle filled with CPC Light Blue. The CTA inside is white and set in lowercase Trade Gothic Bold Condensed.

The space surrounding the CTA should be equal to one X-height on the top and bottom, and two X-heights on the left and right.

The rounded corners should be scaled according to button size. This example shows a corner radius of 14px at 350px wide.

Examples

Print Ads

This style is characterized with the product sitting cleanly on a wireframe background against white. The headline is Trade Gothic and in CPC Light Blue and Dark Gray.

Body copy is Trade Gothic Light in either CPC Light Gray or Dark Gray, depending on the wireframe background. The rest of the copy should follow the standards mentioned in the typography section. Type should be left-justified and end near the furthest edge of the product.

URL and CTA should be set in Trade Gothic Condensed with the URL in CPC Light Blue. The URL should fall under the logo in the bottom right corner of design. If there is a specific CTA to a vanity URL or other external website, the URL should be placed in the body copy.

Print Ads Example

Examples

Ads with Photography

All photography is against a white background with an engineer handling a product. A CAD drawing of the product being used should be in the background at no more than 10% opacity and the headline and body copy should follow the same rules as all other type. Use the CPC 4 color logo on the opposite corner of the photo subject.

 

Photography in Publications

Photography in publications should be used without a border. If a border is necessary to denote the edge of a photo, use a .35pt grey line. Images without a border gives a clean look to the layout and complements the photography. Avoid using multiple product photos in one combined layout. If multiple products need to be shown together, a circle element can be used to hold the image. Also avoid using color overlays on photography to keep the integrity of our photography style intact.

© 2026 Colder Products Company®. All Rights Reserved