Matériaux
Plage de pression
Choix de montage
Taille de la terminaison
À valve ?
Stérilisation
Type de terminaison
Option de joint d’étanchéité
Capacité RFID ?

CPC Launches DripFree™ Connectors for Cleaner, More Efficient Printing Processes

High-resolution images available here. 

Arden Hills, Minn. – September 17, 2026 – CPC (Colder Products Company), part of PSG, a Dover company, and a leading manufacturer of connection technologies used in liquid cooling of electronics, has introduced the DripFree™ Series, a line of non-spill connectors designed to support fast, clean, and efficient servicing of ink delivery systems within commercial inkjet printers.

“The ink spills, waste, and contamination that the printing industry has tolerated during  equipment start up and maintenance can be a thing of the past with the DripFree Series,” said Mat Stahl, Senior Product Manager, CPC. “DripFree Series connectors enable both quick material fills and equipment serviceability, but what really sets them apart is a new lubrication-free design.”

Quick disconnects typically rely on lubricated O-rings. The DripFree Series’ lubrication-free valve avoids the risk of contaminants from lubricants that can enter the flow path and affect print quality. The new technology enables thousands of non-spill disconnect cycles without the need for lubrication.

The DripFree Series also features non-spill valves that help prevent messy ink spills after disconnection. The same valve technology minimizes air inclusion during connection, reducing or eliminating foaming within the ink line. Together, these capabilities support print quality, reduce ink waste, and help keep printing environments clean.

The DripFree product line is manufactured in an ISO Class 8 cleanroom, minimizing particulate generated during assembly. The connectors are chemically compatible with a wide range of inks and solvents, and ergonomic thumb latches make connections and disconnections fast and easy.

The first size in the DripFree Series is a compact 1/8" flow quick disconnect, the DripFree™ DF2 Series*, which fits conveniently into tightly configured printing systems. For more information on the DripFree DF2 Series, click here.

CPC will showcase the DripFree Series at Booth N6206, PRINTING United Expo, Sept. 23-25, in Las Vegas.

For more information about CPC’s portfolio of connectors for print and ink management applications, visit cpcworldwide.com/print-and-ink.

*DripFree™ DF2 Series spillage per disconnect is <0.05mL, less than a drop of water.

###

About CPC

CPC (Colder Products Company) is a leading provider of quick disconnect couplings, fittings and connectors for thermal management (liquid cooling of electronics), life sciences, biopharma, industrial and chemical handling markets. During its nearly 50-year history, CPC has built a portfolio of more than 10,000 connector products. CPC is a business unit of Pump Solutions Group (PSG), an operating company within Dover Corporation.

Editorial Contact:

Matt Hareldson, Senior Marketing Strategy Manager, CPC
Tel: +1 612-459-6279
Email: matt.hareldson@colder.com